AnsweredAssumed Answered

Differences between AD9371 and AD9375?

Question asked by tcachat on Apr 17, 2018
Latest reply on Apr 18, 2018 by Vinod

According to AD9375 FAQ the only differences between AD9371 and AD9375 is that the later has extra capabilities: DPD, VSWR measurement and CLGC (Closed Loop Gain Control). If we do not use these extra capabilities, is it true that everything that can be done with the AD9371 can also be done with the AD9375, exactly the same way? In particular, using the same configuration the output level should be the same? On the whole frequency range?

Thank you

Outcomes