AnsweredAssumed Answered

LT1328 Pulse Position Modulation

Question asked by Yuya on Apr 16, 2018
Latest reply on Apr 17, 2018 by Yuya

Hi,

My customers are considering using LT1328.
So I got a question.

 

This is about the Input pulse when communicating at 4 Mbps.

 

# 1   In the image of the oscilloscope shown in Fig. 4, "10"(DATA BIT PAIR) appears for input "1000"(4ppm DATA

  SYMBOL), but is this idea right? (Image below)

  It seems to be different from the table of 4 ppm DATA SYMBOL & DATA BIT PAIR.

  The output data is determined at a position of 125 ns in a period of 500 ns, right?

 

Best Regards,

Yuya

Viewpoint of my pulse position modulation

Outcomes