AnsweredAssumed Answered

Bit rate of FMCDAQ2

Question asked by yzzhsx123 on Apr 15, 2018
Latest reply on Apr 17, 2018 by yzzhsx123

      Hello, guys, recently I am using ADFMCDAQ2 to transmit data. The sampling rate of DAC and ADC are both 1GHz, the maximum signal rate I can set through IIO-Oscilloscope is 500MHz, so how can I check out the bit rate of DAC or how can I calculate it out if I  I load the file through DAC Buffer Input option?

 

Thank you !

Outcomes