AnsweredAssumed Answered

How long should a magnitude ratio remain constant in an AD8302?

Question asked by chamathkv on Apr 15, 2018
Latest reply on Apr 16, 2018 by jdobler

I want to run frequency sweeps from a signal generator where the incident and reflected signals are coupled and sent to the AD8302's two input pins. Is there a certain time period for the AD8302 to provide uninterrupted analog outputs? Suppose I transmit a frequency sweep from 100MHz to 500MHz at 50MHz shifts, where each frequency remains still for about 50ms. Is that time span adequate? Should there be a longer time duration before going to the next frequency?

Outcomes