AnsweredAssumed Answered

Can AD24000 survive ultrasonic bath? 

Question asked by wlummis on Apr 11, 2018

The device is mounted to a pcba which is in turn mounted to a radel housing with 2mm wall thickness.  Should the pcba be mounted on vibration isolators, or is direct connect to molded bosses ok?  Device will be subjected to medical ultrasonic cleaners with frequency range from 40kHz - 132kHz for 10 minute cleaning cycles.  Maximum temperatures are low, 120°F max.

Outcomes