AnsweredAssumed Answered

How to connect AD9528 Eval to AD9234 ADC

Question asked by NilsMinor on Apr 11, 2018
Latest reply on Apr 19, 2018 by NilsMinor

Hi,

 

I have the following setup:

AD9234-1000 Eval Board

AD9528 Evalboard

ADS7-VEEBZ

 

I need to test the AD9234 ADC for next development steps. I need some help in connecting the clock source from the AD9528 Eval to the AD9528 Clock generator. What outputs of the AD9528 should I use diferential or single line? And what setup do I need LVDS or HSTL?

 

The ADC Eval Board has no Clock on it like described in the Wiki but do I also only need to supply 1 GHz to REF Clock and Sample Clock? (https://wiki.analog.com/resources/eval/ad9680-1000ebz ) What about the amplitude  of the clock signal? I can not change the output of the AD9528 Board.

 

I also have problems by accessing the AD9234 via SPI while trying to upload an cfg file. I only have a cfg file for AD9680 is it the same?

 

Thanks

Nils

 

 

Outcomes