AnsweredAssumed Answered

questions about the 9833 output

Question asked by MarkFredette on Dec 9, 2011
Latest reply on Dec 15, 2011 by MarkFredette

Two questions...

 

1. for sin outputs, what is the peak2peak amplitude I should expect? Will the min peak be 0 volts and the max peak be 0.65? Will this depend on output frequency?

 

2. figure 1 in the 9833 spec (rev D) shows a switch from 200 ohm to gnd. I am thinking this really should be in series with the unlabeled buffer output. I mean, the 200 ohm is always connected from output to gnd, no?

 

thanks,

 

mark

Outcomes