AnsweredAssumed Answered

AD9148-EBZ - FMC Adapter, Latency

Question asked by Christof on Apr 10, 2018

Hi everyone,

 

Here it says that the AD-DAC-FMC is (only?) compatible with DPG2 daughter boards, whereas the AD9148-EBZ is DPG3 compatible. Comparing the Schematics of both boards I cannot see any reason why the AD9148-EBZ and the AD-DAC-FMC should not be used together to connect to a FPGA board with FMC connector?

 

The AD9148 is specified to have at least 64 cycles latency. The latency is referred to which clock? f_DAC or f_data?

 

Thanks in advance,

Christof

Outcomes