AnsweredAssumed Answered

What is LMFC period when use fsx4 mode for AD9208?

Question asked by Tim_Sun on Apr 9, 2018
Latest reply on Apr 9, 2018 by Tim_Sun

When AD9208 uses fsx4 mode,5 ADC samples are packed int 4 16-bit JESD204B samples to create a 64-bit frame. In this mode,link parameters are L=8 M=2 F=2 S=4 N=16...

SYSREF period must be an interger multiple of the LMFC, the datasheet says LMFC=ADC clock/SXK

My question is :the value of S shoud be 5 or 4?I think it should be 5,am I right? What about value of K?

 

Thanks

Attachments

Outcomes