AnsweredAssumed Answered

ADCMP580 Hysteresis

Question asked by Yuya on Apr 6, 2018
Latest reply on Apr 10, 2018 by Yuya

Hi,

I would like to use ADCMP580.

So, I have a question.

 

#1 What is the maximum hysteresis?

 

In the text of Datasheet P.14, the maximum hysteresis is stated as ± 70 mV.

The following text will be quoted.
" The maximum range of hysteresis that can be applied by using this method is approximately ±70 mV. "

 

However, looking at Figure 28, since hysteresis is 70 mV, I think that it is ± 35 mV.

 Is "± 70 mV" in the text a mistake?

ADCMP580 Figure.28

Best Regards,

Yuya

Outcomes