AnsweredAssumed Answered

AD8479 - Is the Common mode of +/-900V in the absolute max section depended on the supplies?

Question asked by francisco on Apr 5, 2018
Latest reply on Apr 10, 2018 by francisco

Hi,

 

  About the AD8479:  In the absolute maximum section, it is written that the chip can withstand a input common mode of +/-900V for 10 seconds. Is this 900V depended on the +/- supplies like the +/-600V? If it is do you have a figure similar to figure 11 in the datasheet that would show the 900V common mode vs output voltage and dual supplies?

 

Thanks,

 

Francisco

Outcomes