AnsweredAssumed Answered

ADF4002    MUXOUT function

Question asked by Alexius.KAN on Apr 5, 2018

Hi, dears!!!

The question is about SERIAL DATA OUTPUT of MUXOUT.

Is it the same waveform as DATA pin draws or it appears only after the input shift register is filled?

In other words, can I control two different devices using DATA, CLK and one LE, simply connecting DATA of second device to MUXOUT of the first (CLK and LE are common)? And total cogeword consists of cogeword of first device followed by cogeword of second device  (in a one LE). Of couse I understand that I have to turn on SERIAL DATA OUTPUT of MUXOUT in the first device.


Best regards!

Alexius.

Outcomes