AnsweredAssumed Answered

Design Help FMCOMMS3 , ADRV9361-Z7035

Question asked by FRK on Apr 5, 2018
Latest reply on Apr 5, 2018 by Vinod

I would like to discuss one of my approach regarding AD9361.

I have two option .

1- I have Xilinx VC707 and FMCOMMS3-EBZ . I have built the reference design using Xilinx Vivado and also modify reference design for generation of 20MHz bandwidth . The issue is that I need a host processor for selecting desire tab(selecting bandwidth , Gain etc etc ) on IIO Oscilloscope . I need your guidance that how i can modify (http://analogdevicesinc.github.io/no-OS/ad9361_8c_source.html ) or what should i do that whenever I power On the setup (FMCOMMS3-EBZ + VC707 ) . the setup automatically generate 20Mhz . So i be able to run without a host processor .

 

2- I have also ordered ADRV9361 (ad9361-Z7035) . built reference design provided by Analog Device and also included my own logic for generation of certain bandwidth. Now i need your guidance that how to change source code ( .c ) for making it able to run it without any host processor .

 

Thanking you in anticipation .

 

warm regards

Outcomes