AnsweredAssumed Answered

[ADE9000] Communication was not established with the IC.

Question asked by ybsl on Apr 3, 2018
Latest reply on Apr 8, 2018 by Gary.Kang.AnalogDevices

Hello.

There is a problem using ADE9000 Evaluation Board.

When measuring, i always use ADE90xx EVALUATION SOFTWARE.

Until a few days ago, I was using it well.

But today, I can't connect the ADE9000 to a PC.

The following message appeared.

--

Communication was not establiched with the IC. Check the following:

1. Is the evaluation board powered up correctly?

2. Is the SDP board firmly attached to the evaluation board?

After verifying the above two conditions, re-run the software.

--

I already verified the above two conditions. But the problem is still ongoing.

I want a solution to this situation.

If possible, I want to know which device is down on the Evaluation Board.

Thanks.

Outcomes