AnsweredAssumed Answered

Problem with sequencer of AD7689

Question asked by khal on Dec 8, 2011
Latest reply on Dec 15, 2011 by maithil

Hi,

I have an AD7689 chip which I am programming to sequence between 8 channels through and SPI-DMA setup via a BF592 processor. I built the front end analog and conneted the digital control lines. When I set the seuqnecer of the AD7689 to sequence between channel 0 and 1, I get the output that I expect (i.e. have the correct data in the DMA buffer that I have setup). When I switch between channel 0 and 7, I start getting rubbish data.

 

Has anyone had such a problem. Do you have any code the fixes this issue?

 

Khal

Outcomes