AnsweredAssumed Answered

the problem of ADR3430

Question asked by kevin_pan on Apr 2, 2018
Latest reply on Apr 17, 2018 by kevin_pan

Hi,

My problem is as  follow,

The output of ADR3430 connect to the ADC reference voltage high of MCU,

The enable of ADR3430 connect to the I/O of MCU via a 1K pull_down resistor,

The  VIN of ADR3430 connect to the power of 3.3V,

When the power of 3.3V is turned on, the enable is always pulled down for 30ms or more  and then pulled up. The reference source output is normal?

Is there any requirement of time sequence about the VIN  PIN and Enable PIN while the power on and power off?

Thanks!

Attachments

Outcomes