AnsweredAssumed Answered

Matlab libiio (AD9361) only transfer and receive IQ data

Question asked by Quamstar on Mar 29, 2018
Latest reply on Apr 1, 2018 by travisfcollins

Hi,

 

I'am currently evaluating the matlab support for configuring, transfer and receive data from matlab to the AD9361. So far I understand the examples (fmcomms2/3 streaming example). I was wondering if there is a function that only transfers the IQ data without setting the configurations of the AD9361 (e.g. LO-Freq or Gain). I was monitoring the voltages and currents of the fmcomms3 and have seen that with any function call of stepimpl there is a drop of the current (like you are re-init the device). Funny thing is, that this does not happen when I run the simulink example.

 

So i would like to avoid setting the device configuration all the time when i call the stepimpl function and just want to send IQ data and receive them

 

Kindly regards

Jan

Outcomes