AnsweredAssumed Answered

Power supply for the ADAU1701-MINI evaluation board

Question asked by cmoreno_uw on Mar 28, 2018
Latest reply on Mar 29, 2018 by KJBob

I'm connecting a USB audio device that outputs I2S (the Texas Instruments PCM2707C) to the ADAU1701 (the evaluation board).  I have a simple SigmaStudio project that routes directly.  I connect my headphones, and sound is there.

 

However, when I unplug the USB cable from the USBi and power the ADAU1701 board with a 5V power supply (through connector J2), sound goes away.  I have written the compiled binary to E2PROM, and in fact, it does work even if I do not have SigmaStudio open.

 

The LED (I guess D3) does light up when I plug the power supply to J2.

 

Anything else I need to do?  Unplug the header that comes from the USBi?  Jumpers J3, J1?

 

Thanks,
Carlos
--

Outcomes