AnsweredAssumed Answered

ADF4351 and Frequency Tolerance: We are prototyping a new design with the ADF4351 and a 228ppb TCXO. How do I know I will achieve the 1ppm stability the FCC requires of my design at 860MHz?

Question asked by Henrykw on Mar 28, 2018
Latest reply on Jun 1, 2018 by kpeker

The FCC requires that radio boosters must maintain the frequency stability in the Part 90.213 specification. 

That number is as low as 1ppm at 860MHz. Will the DDS and 228ppb TXCO combination above maintain that stability? 

Outcomes