AnsweredAssumed Answered

How to change AD9375 device clock using the filter wizard 

Question asked by gulesin on Mar 28, 2018
Latest reply on Apr 1, 2018 by sripad

I've been trying to change the device clock  from 122.88 MHz to 125 MHz. Since I have to work with a 10 MHz reference clock. I changed the 122.88 MHz VCXO with 100 MHz VCXO (Crystek Corp.) to get 125 MHz device clock. 

I changed the  PLL2 divider parameters like M1 = 4 N2 = 35  chDIV = 7 in profile generated by the filter wizard but it did not work. Could you please help me on how I changed the device clock? Should I change the parameters given in the source codes or should I use the filter wizard?

 

Regards,

Outcomes