AnsweredAssumed Answered

Arbitrary Waveform Generation and Reception with AD9371

Question asked by UCSD_PSG on Mar 27, 2018
Latest reply on Apr 1, 2018 by sripad

Hi,

 

I would like to use the ADRV9371 (with EVAL-TPG-ZYNQ) as Tx/Rx for arbitrary waveforms.

 

For example I want to generate a RRC 5 MS/s 64-QAM signal in MATLAB, synthesize it and upconvert it using the Tx of the AD9371, then connect the Tx to the Rx, downconvert it, capture the received waveform, and then process the captured data in MATLAB.

 

Is this possible with the AD9371, or should I use a different solution like the AD-FMCDAQ2-EBZ?

 

Additionally, what is the difference between the AD9371 and 9375?

 

Thanks!

Outcomes