AnsweredAssumed Answered

AD9208 clock source

Question asked by Anjan on Mar 26, 2018
Latest reply on Mar 26, 2018 by UmeshJ

Hi,

We need the following details about the AD9208 ADC:

1) What is the best clock source that is recommended for AD9208? we are planning to use 4 AD9208 ADC in a single PCB. All these ADC's required to be synchronized. what is the best method for distributing these clocks to all 4 ADCs?

2) Should we use the same clock source for generating the Device clock(3 GHz) and the sysref, If yes kindly suggest the best part.

Outcomes