AnsweredAssumed Answered

Implementation of H.264 encoder in blackfin DSP:regarding

Question asked by Sathee_bai on Mar 24, 2018
Latest reply on Mar 27, 2018 by Raj

Sir,

 

       I have the following queries.

1. Do you have full assembly code of H.264 encoder baseline profile with full documentation.

2. Is the code developed by AD capable of compressing SD resolution @ 25/30fps.

3. What is the Blackfin processor u r suggesting for this application.

4. What is clock rate at which the processor has to be operated to do this application of encoding SD resolution @25/30 fps as per H.264 baseline profile.

5. Where do you store reference frames.

6. With Blackfin DSP what are the peripheral devices required to meet the requirement.

Thank you in advance

Outcomes