AnsweredAssumed Answered

Output video resolution and frequency of ADV7611

Question asked by Ather on Mar 22, 2018
Latest reply on Mar 26, 2018 by GuenterL

Hello all,
I want to convert hdmi video to VGA using CN0282 converter. My input video will be of resolution 768 x 576 @ 50 Hz. By looking at the table of prim_mode and vid_std I don't find this video standard however I can use free run mode and set horizontal or vertical thresholds  so that it does not enter in free run mode. 

My question is whether am I right that it will not enter free run mode in this case ?

Also if this the case, then what will be the output resolution and frequency of the video ? (Either that is coming from hdmi port or the one which is set using prim_mode nad _vid_std) ?@

Outcomes