AnsweredAssumed Answered

What is the maximum data rate of AD9684 when operating in parallel interleaved mode?

Question asked by torry on Mar 20, 2018
Latest reply on Mar 23, 2018 by TonyM

In the datasheet, Figure 5 depicts the parallel interleaved mode and the caption says  "output sample rate < 625 MSPS".  Does this mean 625 MSPS for each channel?   Or 625 MSPS for both channels combined (ie 312.5 MSPS per channel)?   I assume that since it is a Dual 500 MSPS converter that it can be run at 500 MHz and get both channels data out of the chip.  I just wanted to double check before proceeding with the design.

 

From the datasheet...

 

Outcomes