AnsweredAssumed Answered

AD9375 has BW minimum of 8 MHz in the Rx that would limit the sensitivity of the receiver. Now if I am interested to use it for 1.4MHz LTE signal how can I make sure that the receiver can sense this ?

Question asked by mayank_design on Mar 20, 2018
Latest reply on Mar 20, 2018 by travisfcollins

For AD9371/AD9375  :

Lets say I have a Receiver with minimum bandwidth of 8 MHz .

For LTE the minimum BW is 1.4 MHz .

 

So is it right to say the minimum detectable signal of the receiver will not be able to detect the LTE 1.4 MHz and 5 MHz BW since it is below the noise floor of the RX?

or , is there a way I can use the RX to detect the 1.4MHz band.

Outcomes