I am using an ADV7481 that connects via MIPI to an i.MX6 (running Linux) over 4 CSI lanes. I am attempting to set up the ADV7481 for HDMI input, YUV 422 8-bit, 4-Lane CSI output. I originally posted this question in the video forum, but it was suggested I post here for better answers.
I am using the “:08-08 Free-run MIPI TxA CSI 4-Lane - YUV422 8-Bit, 1280x720p 60Hz:” snippet from the ADV7481ES3C-VER.3.6c.txt file for the ADV7481 required settings in order to generate a test pattern (colorbars) over the MIPI connection to the i.MX6.
I can communicate with the part successfully, and can program the EDID successfully (verified with a GoPro camera hooked up to it), so I know communication is good between the i.MX6 and ADV7481.
However, when I capture the test pattern, it has obvious defects. I’m not sure what it could be, but I am also unsure what the color pattern is actually supposed to look like at this resolution. I have attached a screen grab of the test pattern I am getting.
Looking at the binary data for this raw video capture, the format actually looks like yuv420, not yuv422, which is very strange. The settings are clearly yuv422 going to the ADV7481, so this is the most important issue to resolve at first. Why am I receiving what appears to be yuv420 back? I am using ffplay (from the ffmpeg project) in order to play the raw video capture, and it claims that the color format is also yuv420 when it attempts to discover the format automatically. This software has been used to view other video captures in yuv422 format, so I trust it is not being faked about the format.
Command line to run raw video file:
ffplay.exe -f rawvideo -pixel_format yuv420p -video_size 1280x720 test-color-bars-1280x720-yuv422.yuv
Another developer analyzed the binary data when I ran the same script (except set for solid blue screen instead of color bars), and he also concluded that the format was actually yuv420 instead of yuv422:
“Looks like YUV 4:2:0 (https://en.wikipedia.org/wiki/Chroma_subsampling)
I see 0x0f for the first 0xe1000 bytes(0xe1000 == 921600 == 1280*720)
0xC4 for the next 0x38400 bytes(0x38400 == 230400 == (1280 * 720 / 4))
0x75 for the next 0x38400 bytes
”
I have attached both the color bar raw video file, and the solid blue raw video file in separate zipped attachments.
In summary, I’d like to know what the colorbar pattern should actually look like given the setting from that script, and why the received format appears to be YUV 420 instead of YUV 422 like the script is attempting to set up in the ADV7841.
Thank you for taking a look!
Hi,
Like you said here this question is not specific to Linux, so we can't really help much with it.
But be aware that the imx6 allows for format conversion in their image receive and processing chain. So the data that is received over the MIPI link is not necessarily the data that is stored in the memory buffers. Make sure the the imx6 is configured to store the data in 422.
- Lars