AnsweredAssumed Answered

Is LTC4413-1/LTC4413-2 Can detect the Input Power Source automatically

Question asked by sr.sr on Mar 19, 2018
Latest reply on Mar 22, 2018 by DEddleman

Hi,

I am using this LTC4413-1/LTC4413-3 for the multiple input and single output application to get single power output from multiple one. Now i want to detect that how many power sources are connected to the IC, to select one from them.  

I want to know that is this IC LTC4413-1/LTC4413-2 can DETECT the power input sources.

I am using this IC for multiple power source input DETECTION and SELECTION.

So, is this feature is available in this IC or not.

 

Thanking You

SR

Outcomes