AnsweredAssumed Answered

LT8650S using dual channel different output cyrrent

Question asked by kamino-t@tecstar.macnica.co.jp on Mar 16, 2018
Latest reply on Mar 21, 2018 by kamino-t@tecstar.macnica.co.jp

Hello

 

Is it possible dual channel using below condition?

Are there any problem?

 VIn range 5.8 to 39V

Vout1 3.3V 2.5A

Vout2 5V 5A

 

In the datasheet

"Both channels are designed for output currents up to 6A,
but thermal considerations practically limit the output
currents to 4A of continuous current from each channel
simultaneously."

 

Are there limiting circuit?

 

 

Best Regards

T.Kamino

Outcomes