AnsweredAssumed Answered

AD9371 with ZCU102 board - AD9528_initialize() failed

Question asked by Rahul1004 on Mar 16, 2018
Latest reply on Mar 19, 2018 by Rahul1004

At initialization I am getting the following on the UART:

   Please wait...

   AD9528_initialize() failed

 

I have checked the register address values of AD9528 :

 

1) 0x010A = value is 0x00 

 I am writing the value 0x2 but when i read back the value its value turn out to be 0x00.

 

2) 0x0508( Readback 0 )  = value is 0x21

which means my PLL1 is locked but PLL2 is not locked

 

I have also checked the clock which is generated by AD9528 "  FPGA_REF_CLK+ and DEV_CLK_IN+ " but no clock is generated at output.

 

Was there anything else that needed to be modified in the code to initialize it ?

Outcomes