AnsweredAssumed Answered

ADRV9371 HDL reference directory structure, documentation

Question asked by centercitybill on Mar 15, 2018
Latest reply on Mar 22, 2018 by CsomI

We are designing a custom board using the AD9371. We are using an onboard processor running Linux to configure the AD9371 via the SPI port. We are also developing an Xilinx Artix FPGA to interface to the AD9371 JESD204B interface. My question is in regard to using the HDL reference design. I only want to use specific pieces of the reference design. Is there a reference that lists the directory structure of the code so I can figure out what pieces I need to use. If you refer to the block diagram in the ADRV9371 HDL reference wiki I am specifically interested in the AD9371 IP block and the JESD204B interface block.  I have built the code into a local repo using the HDL reference wiki, however I am having difficulty navigating all of the directories that are included in the HDL reference to find what I want to keep. Thanks.

Outcomes