AnsweredAssumed Answered

ADAU1442 ASRC won't work at 192kHz 

Question asked by jtuomy on Mar 13, 2018
Latest reply on Apr 2, 2018 by tuomy

   I have a new product that uses the ADAU1442 running at 48kHz.  The OEM that is building the hardware is having trouble with the ASRC handling of 192kHz signals on BOTH the S/PDIF and the TDM-4 input paths. There is no problem on either path with 44.1,48, or 96kHz signals. Could this be a problem with the ADAU1442's Clock rate? Or should I be looking in the hardware setup registers?

Any thoughts would be appreciated!

Thanks!

Outcomes