AnsweredAssumed Answered

How to give RF(within 70 MHz to 6 GHz) signal as input (RX) to AD9361 and route that RF(mentioned) to one of its output port(TX)? 

Question asked by tancarrerece on Mar 13, 2018
Latest reply on Mar 15, 2018 by Vinod

Hello researchers and engineers,

I'm working on a platform which consists of Zynq 7006 AP SoC and FMCOMMS5-EBZ, my requirement is to give an RF signal from a suitable source(preferably from a signal generator) on one of the ports of the AD9361 transceiver and route that signal to one of its output ports so that an antenna can receive that signal. If it is possible then in which way I should proceed so that I can successfully implement the design? It will be really helpful if I get any small info regarding this.

Thanks,

Tanmoy Das

Outcomes