AnsweredAssumed Answered

ADSP-21469 not booting after being programmed

Question asked by JRyall on Mar 9, 2018
Latest reply on Mar 19, 2018 by Jithul_Janardhanan

I programmed my ADSP-21469 EzKit successfully using the CLDP and an ICE-1000. I set the loader file up to program the parallel flash memory. The command line reported that the programming was done. I set the boot switch (sw4) to position 2 for booting from the parallel flash memory. Then I reset my board.

 

Unfortunately it seems that either the program didn't take, or the board isn't booting. I'm not sure what the problem is but the program runs fine when I run it though CCES and the emulator, but I just can't seem to get it to run on it's own. Any help you can give me would be much appreciated.

Outcomes