AnsweredAssumed Answered

AD9364 products Tx single-carrier with a lot of clutter and low transmitting power.

Question asked by Jess-J on Mar 9, 2018
Latest reply on Apr 10, 2018 by Jess-J

Hi,

I am debugging the AD9364. AD9364 provides a 800MHz LO, and FPGA provides a 1MHz data single from BBP. I aim to get a 801MHz Tx single-carrier. Two problems occured.

 

One is the transmitting power I  get is -12dBm with 19dB attenuation, but get -34dBm with 0dB attenuation. Why I set up larger attenuation and get a  larger power?

 

The other is the spectrum of the Tx single is mussy, with a lot of clutter. I provide a picture attachment.

Outcomes