AnsweredAssumed Answered

Error generating custom BSP for hdlcoder

Question asked by DrMurad on Mar 8, 2018
Latest reply on Mar 21, 2018 by DrMurad

Hi all,

I am using MATLAB 2016b and Vivado 2015.2.1

Started with a simple 'hdlcoder_led_blinking', I can successfully create a vivado project and use hdlcoder to add an led_count ip and run it on the hardware (PicoZed).

 

Then, I wanted to use a vivado project (that we successfully used before and generated .bit file in the Vivado with no errors) as the BSP to the hdlcoder.

 

The attached document shows the errors I am getting. Basically, hdlcoder somehow is not able to locate the required source file. I also show the 'plugin_rd.m' file used.

 

Could you please help me figure out my problem

 

PS:

- if I add the missing files (system_top.v and ad_iobuf.v) to the project, the project works ok and I can generate the .bit file...but I want to stay in the MATLAB environment and do all settings from there.

-I can attach the full folder of the project if needed

Regards,

 

Murad

Attachments

Outcomes