AnsweredAssumed Answered

ADP5300 : Default mode

Question asked by Guillaume76 on Mar 6, 2018
Latest reply on Mar 9, 2018 by Guillaume76

Hello, 

 

I have a question regarding the default state of the SYNC/MODE pin ot the ADP5300 : is there an internal pull down/up resistor to force a default mode ?
This is to know the mode of the IC when the board is powered in order to flash the mcu firmware (by default mcu gpios are configured as inputs, high impedance).

If there is no internal pull down/up then it would perhaps be better to add an external one.

 

Thanks

 

Guillaume

Outcomes