AnsweredAssumed Answered

LT8429 Charger Battery Voltage

Question asked by vic2000 on Mar 6, 2018
Latest reply on Mar 7, 2018 by vic2000

I'm using the DC2069A kit that has the LT8490 battery charger for solar panel applications. LT8490 data sheet shows the battery range from 1.3V to 80V.

The kit is configured to charge a 12V battery. I need to charge either a 24V or 26.4V. I read the LT8490 document but I'm still not sure which resistor(s) should I use in order to change the battery voltage.

I'll appreciate if somebody will give suggestions.

Outcomes