AnsweredAssumed Answered

does Frequency Multipliers work with short chirp signal?

Question asked by zxzhaohui on Mar 5, 2018
Latest reply on Apr 9, 2018 by MRichardson

We are currently considering to use a HMC445LP44 to multiply a short chirp signal with X16.

 

The input signal is a pulsed chirp signal with 1~10 microsecond length and center frequency of 650MHz, and the chirp rate is high (~1.5MHz/us, up to 1.5MHz/ns) and is nonlinear form (means that the instant frequency is not a straight line). The instant frequency is within the working range of HMC445LP44.

 

Will the  HMC445LP4 work with such type signal?

Outcomes