wiktorjunior

AD-FMCOMMS3-EBZ + Zedboard, data transmission directly from FPGA register

Discussion created by wiktorjunior on Mar 5, 2018
Latest reply on Mar 12, 2018 by AdrianC

Hello everyone.

I am working on device which receive and demodulate FM signal, then audio samples are going through FPGA to perform  some realtime DSP on it, after this I want to modulate and transmit audio back again using other FM frequency.

 

I modified custom HDL design to bypass audio output. Now I have signal after DSP on both zedboard audio outputs and  48kHz samples on AXI register to which I have easy access from Linux running on zedboard.

 

Is there any easy way to FM transmit data from AXI register?

 

I tried transmission directly from audio drivers(It's easy to make that kind of audio source in gnu-radio). I connected output and input by jack cable but it resulted huge delays. There was no way to make audio playback using software. I tried to make virtual sound cards, modify settings in pavucontrol, JACK(tons of errors using it) etc.

Also I tried to modify that method: Simple FM transmitter using gnuradio - Opendigitalradio  but there were much bigger delays and corrupted signal.

Next idea was to modify "AD9361_iiostream.c" file, but I am not sure how to prepare audio samples to send. I got repeated silent breaks in transmitted signal.

Btw. Each time I received signal and transmitted something at the same moment, I got overruns and underruns while moving the cursor or open some other apps.

 

Regards, Wiktor

Outcomes