AnsweredAssumed Answered

Video recording and replaying Upto 2k*4k

Question asked by ankurtez on Mar 1, 2018
Latest reply on Mar 26, 2018 by GuenterL

Hi,

I am working on a project to record and replay of video(upto 2k*4k resolution). Video input is from DVI/HDMI. I need a HDMI/DVI splitter ic(1 in 2out) ,one output will be connected to a monitor and other will go to a processor for further processing. The data(DVI/HDMI) coming out from the splitter should be converted to a form which can be an input to the pci e bus of the processor.

So, i require 2chips one is a splitter and other converter ic which can be connected to pci e bus of the proceesor.

How to do this? Is there any chips available? Or should i use a different technique?

Thanks and regards

Ankur

Outcomes