AnsweredAssumed Answered

Data format to and from the Mykonos 9375 JESD links

Question asked by RyanSw on Mar 1, 2018
Latest reply on Mar 2, 2018 by sripad

Hello,

 

I am trying to do a loopback test within my FPGA in order to test some custom DSP blocks.  I am having trouble figuring out the data format that is required for the deframer and what is coming from the framer.

 

I have read in the user guide that the DAC has 14bit resolution and that the upper 14 bits of the I and Q sample are used [15:2] and the lower 2 bits are unused [1:0].  Is this correct, can I just pad bits 0 and 1 with zeros?

 

My other question is regarding the framer.  It looks like the ADC has 16bit resolution, is this correct or is the same as the DAC and I need to use upper or lower bits?

 

Thanks

 

Ryan   

Outcomes