AnsweredAssumed Answered

question about ADV7619 and ADV7842 API source code packages

Question asked by WilliamLian Employee on Feb 28, 2018
Latest reply on Mar 5, 2018 by PoornimaSubramani

One  customer will use ADV7842 and ADV7619 in a system, they need the API source code, by ADI website, customer got two source code package, the ADV7619_API_Library-Rel1.61.2.1 and ADV7842_API_Library-Rel1.55.2.1,  customer engineer compared the two packcacge, found they're very similar ( similar architecture, just a litter difference in the SRC/RX/HAL subdirectory, there're two folders 4G/ADV7842 and 5G/ADV7619 which including the ADV7842 and ADV7619 configuration)  and seemed the ADV7619_API_Library-Rel1.61.2.1 is newer than the ADV7842_API_Library-Rel1.55.2.1.  Customer want to know what's the relative between the two pacakges? are they compatible? if need one package to cover both ADV7619, whether can use the ADV7619_API_Library-Rel1.61.2.1 and plus the 4G/ADV7842 folder content which from the ADV7842_API_Library-Rel1.55.2.1?

Outcomes