AnsweredAssumed Answered

LTC1856 configuring and reading back differential channels

Question asked by cliver1 on Feb 27, 2018
Latest reply on May 7, 2018 by ghoover

I'm testing the LTC1856 differential channels, Chan 6 & 7. I'm confused how to configure them and read them back.

Both channels work in single ended mode reading back 32767 0x7FFF with +10V input.

When I configure the channels as differential and input +10V on chan 6 and -10V on chan 7 I read back 32767 from both channels. I also get the same result when injecting +5V on chan 6 and -5V on chan 7?

I've configured both channels with the input word 00110000 which should configure the multiplexer for differential channels + on 6 and - on 7.

Outcomes