AnsweredAssumed Answered

Input voltage tuning speed for HMC739LP4 evaluation board?

Question asked by Nagarjun on Feb 26, 2018
Latest reply on Jun 7, 2018 by MRichardson

Hi, I have a HMC739LP4 evaluation  board, which I want to use to setup a heterodyne phase locked loop. I wanted to know the fastest speed/frequency or response time, upto which I can tune the input voltage signal ? This is important for me, since I need to know if this VCO is suitable for my application. For e.g. Can I frequency modulate the (input voltage of the) VCO and achieve datasheet performance for a MHz range input voltage signals ? I have a tunable loop-filter that works upto 200 MHz. This information isn't present in the datasheet as far as I understand. Thanks...

Outcomes