AnsweredAssumed Answered

AD5933 Device Tree Patch

Question asked by chrisfrederickson on Feb 26, 2018
Latest reply on Mar 6, 2018 by DragosB

Is there a patch available for device tree support for the AD5933? This was referenced in November 2017 in the post below.

 

Instantiate I2C Device AD5933 

 

We are generating the MCLK input to the AD5933 using direct digital synthesis, as suggested in the AD5933 datasheet, as we need to measure at frequencies lower than what the internal oscillator will allow for. And for our application, we need to be able to change the external clock frequency. I don't presently see any way to do that with the current driver.

Outcomes