AnsweredAssumed Answered

ADV7513 - Pixel repetition Support

Question asked by LalithaaShree on Feb 26, 2018
Latest reply on Feb 26, 2018 by GuenterL

Hi,

   I am using ADV7513 to convert 24 - Bit Parallel RGB input to HDMI Out.

 

   The specifications of input is :

                           PCLK: 9 MHz

                           Resolution: 320 x 426

                           Frame Rate:60 fps

 

   Since the clock frequency is very low, I used Pixel repetition to convert it to match HDMI standard.

 

   I multiplied the clock by 2 and got the HDMI out with resolution 640 x 426.

 

   Is there any way to get the same resolution as input at the output also while using Pixel repetition??

Outcomes