AnsweredAssumed Answered

Setting of AD9361 minimum RF bandwidth

Question asked by weehong.yeo on Feb 25, 2018
Latest reply on Feb 26, 2018 by weehong.yeo

Hi, I referred to AD9361 Minimum channel bandwidth and it states that the minimum analog RF bandwidth is 200kHz.  However I found that I was able to echo values less than 200000 into in_voltage_rf_bandwidth successfully?  Well at least the value is set.  I can set it to as low as 1 Hz?  Shouldn't it throw an error?  Or is it that any value that is less than 200000 is assumed to be 2000000?  

 

Any clarification will be greatly appreciated!  Thanks!

Outcomes