AnsweredAssumed Answered

Manually setting I2C addresses of components in SigmaStudio

Question asked by Reini on Feb 25, 2018
Latest reply on Feb 26, 2018 by mmmike

Hello all,

I wondered if it is possible to set the I2C addresses of components manually in Sigma Studio. In my project I have some DC generators I want to set every 100ms which I have to do with safeloads. But I can only set one DC generator at a time with one safeload. It would be nice to have the option to set three or four components in one safeload, that would spare a lot of I2C hardware transmission time :-) The DSP I use is ADAU1450

Any suggestions?

 

With kind regards,

 

Reini

Outcomes