AnsweredAssumed Answered

HDMI Receiver which supports resolution scaling

Question asked by MaxG on Feb 23, 2018
Latest reply on Mar 2, 2018 by MaxG

Hi,

 

i require a HDMI-receiver (or DVI) Receiver which supports resolution rescaling.

I need to drive a HD-Display (1920x1080) which is connected via dual-channel LVDS. This display needs to support a resolution of 1024x768 and 1920x1080. A 48-Bit Interface instead of LVDS would also be acceptable.

 

The display requires a resolution of 1920x1080 regardless of the HDMI-Signal.

 

If this is done via "stretching" or just dumping the data in the middle or the edge of the screen is not important. I only require readable text for the smaller resoltion, this is used for configuration purposes in some cases.

 

Does the ADV7610 support this?

If not, wich part supports this feature?

Thanks vor any help in advance!

Outcomes